Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Product List
Design of ACAS-AT Components

The ACAS AT design offers significant advantages compared to discrete resistor types. The resistive elements are an extremely stable thin film resistive alloy with meander trimming. The trimming geometry allows the resistor to homogeneously dissipate power and distribute thermal energy across the entire resistive element. This enhances the stability of the ACAS AT components to low resistance drift of ≤ 0.1% after 1000 h load life test by reducing the intensity of single hot spots on the resistive film elements when the resistor is in use.

PTM Veröffentlicht am: