Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Product List
Thermistor Resistor Network Simulation Tool Slide 11

The “Recommendations” tab shows the applicable thermistor/resistor network along with the part number of the thermistor as well as part numbers for the fixed series and/or parallel resistors. In addition, the user can click on the part numbers provided in the “Recommendations” tab and will be subsequently redirected to the pertinent datasheet for that part series. If the computations are repeated and only change the Minimum Average Required Current, it’s likely that the output will recommend different part numbers as shown here. To run again and again simply use the “Reset” button as previously mentioned.

PTM Veröffentlicht am: