Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Product List
Features and benefits LUG01T Datasheet
Among these, Vishay’s featured Lug Thermistor series has some unique characteristics that are highlighted here in more detail. The LUG01T Series provides superior stability at a peak temperature of 150°C. More specifically, its resistance drift (∆R/R25) is specified at ≤±3% after 5000 hours at 150°C dry heat. Another key feature of the LUG01T is its insulation voltage withstanding; a robust rating of 2.7 kVAC. Its durable construction utilizes a tin plated copper ring tongue terminal and a NEMA HP-3, 600 VRMS rated ETFE insulated cable. It can be easily mounted to a surface by means of an M3 screw allowing for a good thermal contact and accurate surface temperature measurement. The LUG01T Thermistor can be manufactured in a number of NTC resistance values and beta curve combinations with tolerances as low as 1%. In addition, the LUG01T is AEC-Q200 Automotive qualified and select configurations are also UL recognized. As with all other Lug thermistors, this series can also be customized to meet specific design needs.
PTM Veröffentlicht am: