Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Product List
LTSPICE-Slide11

The graph shown here highlights the effects of altering the reference temperature which is very useful as each application has its own unique operating temperature range/temperature of most importance. For example, by adjusting the reference temperature and resistance in the PARAMS field of the NTC Thermistor model to a higher nominal temperature point, the resulting output minimizes the voltage variation at higher temperature (i.e. essentially shifting the larger portion of the tolerance to 25°C).

PTM Veröffentlicht am: