Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Product List
Selecting the Best Multi-Sourced Linear Regulator Slide 2

Switching regulators are increasing in use due to the need for higher power efficiency and the desire to make the world green by reducing the carbon footprint. However, linear regulators are sometimes desired due to cost, solution size, or output voltage noise. When input to output differential voltage is small, low dropout (LDO) linear regulators are the default choice. However, standard linear regulators are chosen when input voltage varies widely and low cost and multiple sources are desired.

PTM Veröffentlicht am: