Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Product List
Code Composer Support for the Concerto Line Slide 8

Once the target configuration is launched, notice that each of the two cores of the Concerto device is still disconnected from the CCS debug session. Launching the target configuration actually only connects CCS to the emulator, it does not connect to the cores. That must be done manually, which is the next step.

PTM Veröffentlicht am: