Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Product List
HiDef-Slide18

In sequence mode, the HDO oscilloscopes can capture thousands of trigger events and store them as segments in the instrument’s acquisition memory. This is very useful when capturing many fast pulses in quick succession with minimal dead time, or when capturing few events with long time intervals between them, in which case the lengthy dead time does not waste memory. Each segment is triggered, captured, and stored when the pre-determined number of trigger events is reached. All trigger events are time stamped and displayed to the user.

PTM Veröffentlicht am: