Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Product List
commercial-slide4

SDE technology is a flexible approach to crimp tooling, that allows the use of the same dies on tooling across a range of application platforms. Dies are interchangeable in tools from portable hand tools, manual or battery-powered to pneumatic hand tools and electric bench terminators. It is a family of tools that the customer can take from bench to production or into the field, without the need for dies fitted to each kind of tool. They are ideally suited for R & D, networking applications and on-site maintenance work. Customers can be sure the dies will fit the long-term needs, because they are completely compatible with all tools in the SDE system. They move with a customer as the needs grow.

PTM Veröffentlicht am: