Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Product List
Standard Line of FASTON - Slide2

TE Connectivity (TE) offers a Standard Line of FASTON receptacles providing innovation at the receptacle-to-tab interface and the wire crimp. Over the past 60 years, TE has continued to introduce lines of Quick Disconnects to help reduce insertion forces and improve user experience. The standard FASTON is a line of receptacles to meet the latest customer requirements. This presentation will review the features and benefits of the mating interface of the standard FASTON and look at how the 2D Crimp option may be able to benefit the customers operations. Straight receptacles are offered with F-Crimp or an innovative 2D Crimp, while flags have Tab-Lok or 2D Crimp. 2D allows one terminal to be used with a full range of wire sizes. Other crimp designs require three or four terminals to cover that range of wire sizes.

PTM Veröffentlicht am: