Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Product List
Si100x/1x ISM Transceiver Family Slide 26
Now that it is understood how the system is going to operate with respect to the peripherals and the processing requirements based on each task, the average current can be quantified. Each task has an average current consumption based on the current required to perform the task and the period with which the task is executed. For example, if there is a task that consumes 300µA with a duty cycle of 50% then the average current for that task is 150µA. The total average current consumed can be determined by adding together all of the average currents for each of the individual tasks. Once obtained, this value can be compared to the maximum average current allowable by the system and verify that it does not exceed that value.
PTM Veröffentlicht am: