Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Product List
bsp control
The Board Support Package (BSP) controls the common settings for drivers and middleware. In the example displayed here, a timer running at 20 MHz and a serial communication at 8 MHz. Without the common settings of the BSP, there would be a conflict. This is managed by the BSP and controls the MCU start-up.
PTM Veröffentlicht am: