Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Product List
not prog
Configurable, or multi-function logic, is a logic device that can be “configured” to provide one of several different logic functions in a single package. Configurable logic is not the same as programmable: all devices are identical and do not need to be programmed before use. A more descriptive name might be “PCB Configured Logic” because only the wiring of the circuit board changes the configuration, the device itself does not change in any way.
PTM Veröffentlicht am: