Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Product List Associated Content
12 V and 48 V Application in MHEV

Shown here is the configuration of a mild hybrid car. In mild hybrid cars, there will be two voltage levels, the 12 V and 48 V board nets. The combustion engine is connected to a so-called belt driven starter generator which is connected via a belt. The important point is that there will be an increasing demand for devices for 48 V board nets, and this is where the 80 V RET comes into play.

PTM Veröffentlicht am: