Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Product List
LED-Slide7

Due to the success of the LCD Chip on Glass display, Newhaven Display introduced OLED Glass. OLED Glass comes in a 2 x 16 size and is offered in blue. The OLED Glass display features all the great OLED technology advantages, such as wide viewing angles and extreme temperature ranges. OLED Glass also features a 24-pin FFC connector, parallel, I2C and SPI interface options.

PTM Veröffentlicht am: