Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Product List
PIC24F Curiosity Development Board Slide 8

There are several MikroElektronika Click board demo’s created that support Microchip’s PIC24F Curiosity or Explorer 16/32 development boards. As shown on this slide, these include the ADC, Digi POT, DAC demo’s which use other Microchip silicon. There is also GPS, relay, and microSD Click code available. All of these demos are available for immediate download and the boards can be purchased from MikroElektronika or on microchipDirect.

PTM Veröffentlicht am: