Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Product List
pn build
Displayed here is a breakdown of the part numbers for this series based on the available product characteristics. Starting with the base part number, MAX31875R, the engineer will then select versions 0 through 7 to specify the I²C slave address that is required for the design. Next is the TZS, which denotes the 4-bump wafer level packaging. The plus symbol denotes the lead free package. Lastly, all part numbers will end in T which specifies tape and reel. The orderable part number will consist of fifteen characters.
PTM Veröffentlicht am: