Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Product List
x2y-slide9

There are many advantages to having both Y capacitors present in one device. In addition to the balanced internal electrode structure, the external effects of voltage, time, and aging are equal on both capacitors at all times. Also, the PCB layout for the device is inherently balanced compared to two discrete capacitors. These factors lead to exceptional common mode rejection for EMI filtering applications.

PTM Veröffentlicht am: