Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Product List
running

Now that the evaluation board is configured, the designer is ready to begin the evaluation. Open the “Sensor Evaluation Kit 002” app that was downloaded in the initial setup. Once the evaluation kit is open, select the sensor family and part number to be evaluated and click “Submit”. The designer should now see results from the sensor. Setting up and evaluation of the sensors is really that easy.

PTM Veröffentlicht am: