Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Product List
FH39-Slide5

This slide shows the contact structure of the FH39 series. The FH39 realizes high contact reliability because of two features. First the flexible contact can move like a spring, allowing the contact point to follow the FPC, and second the FH39’s flexible contact can firmly connect with the FPC despite of the thickness which can vary from point to point.

PTM Veröffentlicht am: