Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7
HARTING ix Industrial® - Robust

HARTING‘s ix Industrial® guarantees that the device will function reliably. This is ensured by five robust THR shield contacts which permanently and securely affix the socket to the printed circuit board, thereby preventing damage to the conductor tracks caused by the exertion of high forces on the sockets. The active locking of the socket and connector is achieved using two stable snap-in hooks made of metal, providing clear haptic feedback which confirms a secure connection. The connection between cable sheath and plug connection is engineered in the form of a robust crimp connection. This ensures a perfect and robust interface that even meets the high shock and vibration resistance established in EN 50155 railway specifications, guaranteeing a long service life that boasts 5,000 mating cycles. The ix Industrial is also engineered for full reverse compatibility and integration with existing systems.

PTM Veröffentlicht am: