Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Product List
Sound Location Direction Arrays

Sound location detection microphone arrays are another common array topology which can typically be implemented by placing microphones on the perimeter of a circle or a sphere. Electronic signal processing is then used to determine the desired signal from each microphone, while the relative time delay of the desired signal between each microphone is used to pinpoint the source of the sound relative to the microphone array. This is often used for gunshot detection by the police and military.

PTM Veröffentlicht am:
PTM Updated on: 2021-10-01