Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Product List
A495x-Slide5

A unique feature of the A4952 is the open drain fault output that can be used to notify the user when an overcurrent event has been triggered. In addition the A4952 has a selectable retry feature. If the retry pin is pulled to ground the device will, in the event of a short circuit, turn off the outputs for 2ms before enabling the bridge again.

PTM Veröffentlicht am: