Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Product List
Image of Advantech WISE-2410 LoRaWAN® Vibration Sensor - Key Features

There are four key features of the WISE-2410: it reports VRMS (Velocity Root Mean Square) value per the ISO-10816-3 standard (see previous Advantech vibration PTM for fuller description of ISO-10816), LoRaWAN® provides long range, low power wireless solution, the onboard calculation of both VRMS and eight other vibration values make inspection easier, and finally, two years of battery life with thirty minute reads.

PTM Veröffentlicht am: