Maker.io main logo

SparkFun Qwiic Button Hookup Guide

91

2024-07-09 | By SparkFun Electronics

License: See Original Project Arduino Qwiic

Courtesy of SparkFun

Guide by EL DUDERINO

Introduction

Buttons are a great way to add a tactile input to your project but dealing with pull-up resistors, debouncing, ‎polling, and using GPIO pins for each button can be a hassle. Enter the Qwiic Button (Red or Green) and ‎the Qwiic Button Breakout! These breakouts eliminate nearly all the inconvenience of using buttons by ‎converting everything to an easy-to-use I2C connection using the Qwiic Interface.‎

 

We have three versions of the Qwiic Button available. The Qwiic Button (Red) and Qwiic Button (Green) come ‎with a pre-populated red or green pushbutton with a built in LED to illuminate the button and the Qwiic Button ‎Breakout leaves the button unpopulated so you can choose your own tactile button.‎

Using the Qwiic Button is as simple as sending the command button.isPressed() to check the status of the button. ‎In addition to handling status checks and debouncing, the Qwiic Button has a configurable interrupt pin which ‎can be adjusted to activate upon a button press or click. This allows you to trigger specific behavior or ‎functions in your code when the button is used and frees up processing time that would normally be used to ‎constantly poll a button's state.‎

The Qwiic Button also includes a First-in First-Out (FIFO Queue) which keeps track of when the button was ‎pressed so if you are hosting a game show you can easily keep track of which contestant pressed their button ‎first without needing to constantly poll the buttons!‎

Required Materials

The Qwiic Button requires a Qwiic-enabled microcontroller:‎

And you will also need a Qwiic cable:‎

Or, if you want to use a microcontroller without a Qwiic connector, you can add one using one of our Qwiic ‎Shields, the Qwiic Adapter board, or adapter cables:‎

Finally, if you are using the Qwiic Button Breakout you'll need to solder a button to the board:‎

Realistically, you can solder any pushbutton to the Qwiic Button Breakout so long as it fits the button footprint. ‎We have a couple other options available in our Button Category that will work perfectly with the Qwiic Button ‎Breakout.‎

Heads Up! If you choose an LED Tactile Button, pay close attention to the polarity marks on your button and ‎Qwiic Button Breakout to place it correctly. If the button is inserted with reverse-polarity, the LED will not ‎work. If you are not positive on the polarity of your LED Button, you can use a multimeter to check.‎

ADDITIONAL TOOLS FOR SOLDERING TO THE QWIIC BUTTON BREAKOUT

Note: If you want to use the Qwiic Button Breakout then you will need to solder a tactile button to ‎the board. You may already have a few of these items, so feel free to modify your cart based on ‎your needs.‎

Suggested Reading

If you aren't familiar with the Qwiic system, we recommend reading here for an overview:‎

qwiic_1

Qwiic Connect System

We would also recommend taking a look at the following tutorials if you aren't familiar with them.‎

  • Button and Switch Basics: A tutorial on electronics' most overlooked and underappreciated component: the ‎switch! Here we explain the difference between momentary and maintained switches and what all those ‎acronyms (NO, NC, SPDT, SPST, ...) stand for.‎
  • I2C: An introduction to I2C, one of the main embedded communications protocols in use today.‎
  • Processor Interrupts with Arduino: What is an interrupt? In a nutshell, there is a method by which a ‎processor can execute its normal program while continuously monitoring for some kind of event, or interrupt. ‎There are two types of interrupts: hardware and software interrupts. For the purposes of this tutorial, we will ‎focus on hardware interrupts.‎
  • Qwiic Shield for Arduino & Photon Hookup Guide: Get started with our Qwiic ecosystem with the Qwiic ‎shield for Arduino or Photon.‎

Hardware Overview

Tactile Button

This is a standard pushbutton with a built in red or green LED depending in which version you have. The LED's ‎anode (positive pin) is connected to an I/O pin on the ATtiny84 so you can turn it on and off as well as control ‎the brightness. If you have the Qwiic Button Breakout, you can choose your own color of button from the ‎selection listed in the Introduction of this guide or any tactile button that fits the footprint on the breakout.‎

button_2

Red Tactile Button

button_3

Button Footprint

Heads Up! If you are using a Tactile Button with an integrated LED, pay close attention to the polarity marks ‎on the button and match them with the Diode Markings on the Qwiic Button Breakout. You can use a ‎multimeter to check polarity if you are not sure.‎

Qwiic and I2C Interface

The easiest way to use the Qwiic Button is with the Qwiic connect system. Simply plug in a Qwiic Cable to start ‎talking to it.‎

connectors_5

Qwiic Connectors

pins_6

I2C Pins

Alternatively, you can solder to the I2C pins broken out on the board.‎

ATtiny84‎

The ATtiny84 has pre-installed firmware to handle the various functions of the Qwiic Button. It acts as an ‎intermediary device to send and receive I2C data for things like button presses, clicks, the FIFO queue and it ‎allows you to set a custom I2C address for the Qwiic Button. If you would like, you can modify the firmware on ‎the Qwiic Button using the 2x3 pins on the back of the board. The firmware can be found in the Hardware ‎GitHub Repository and if you need help programming the ATTiny84, check out this tutorial.‎

attiny_7

Jumpers

Note: Never worked with solder jumpers before? Or maybe just need some tips or a quick refresher? Check ‎out our How to Work with Jumpers and PCB Traces tutorial.‎

I2C Address Jumpers

There are four solder jumpers on the board (labeled A0, A1, A2 and A3) you can close to set the I2C address. ‎The firmware reads the logic of each address pin so, by closing multiple jumpers, you can modify the Qwiic ‎Button with up to sixteen unique addresses! If you do not want to use the address pins, the address can also ‎be configured using the ChangeI2CAddress Example from our Arduino Library.‎

  • All Open: Factory or User Set I2C Address: 0x6F (Factory Set) or 0x## (User Set)
  •  Alternate Address Jumpers: Closing an address jumper sets the pin LOW. On boot-up, the firmware ‎checks the state of these four pins and adjusts the I2C address following this logic: 0b0110,A3,A2,A1,A0 For ‎example, with both A0 and A1 jumpers closed, (A0 = 0, A1 = 0, A2 = 1, A3 = 1) the I2C address of the ‎Qwiic Button is set to 0x6C (0b01101100). Check out the table below for a full list of all the I2C addresses ‎and the jumper logic used to set the address.‎

CLICK HERE TO OPEN THE I2C ADDRESS TABLE

table_8

adr_9

I2C Pull-Up Resistors

Severing the trace on the I2C jumper will remove the 2.2kΩ pull-up resistors from the I2C bus. If you have many ‎devices on your I2C bus, you may want to open these jumpers by severing the trace in between the pads.

trace_10

Interrupt Pin

The Interrupt Pin can be used to trigger events on your microcontroller. It is active LOW and can be configured ‎to activate on either a button press (held down) and click (press-and-release). By default, the Interrupt Pin is ‎pulled to 3.3V via a 10K resistor through this jumper. Just like the I2C pull-up resistors, you can open it by ‎severing the trace in between the pads. This may come in handy for low-power projects that do not require ‎the Interrupt Pin.‎

int_11

Board Dimensions

The breakout board is the standard Qwiic size of 1" x 1" and has two mounting holes that fit a standard 4-40 ‎screw.‎

mounting_12

Hardware Assembly

With the Qwiic connector system, assembling the hardware is simple. All you need to do is connect your Qwiic ‎Button to Qwiic-enabled microcontroller with a Qwiic cable. Otherwise, you can use the I2C pins if you don't ‎have a Qwiic connector on your microcontroller board. Just be aware of your input voltage and any logic level ‎shifting you may need to do since the Qwiic system runs at 3.3V.‎

system_13

If you have the Qwiic Button Breakout, you will need to solder a button into place. If you are using a Tactile ‎Button with an integrated LED, remember to pay close attention to the polarity marks on your button and ‎match them to the markings on the top of the Qwiic Button Breakout. If you purchased a tactile button from ‎SparkFun, the anode will be marked with a small "+" on the top of the button.‎

solder_14

Having a hard time seeing the "+" symbol?

Important! Soldering the button into place with the LED backward is not easy to fix. Verify the polarity of your ‎LED prior to soldering into place! You can use a multimeter to check polarity if you are not sure.‎

Once your button(s) are soldered into place and you're certain all pins are well connected, you're ready to go! ‎The image below shows two of the several options for buttons on the Qwiic Button. One is the standard Red ‎LED Tactile Button and the other is from our Multicolor Button 4-Pack:‎

pack_15

Qwiic Button Arduino Library

Note: This tutorial assumes you are familiar with Arduino products, and you are using the latest stable version ‎of the Arduino IDE on your desktop. If this is your first time using the Arduino IDE, please review our tutorial ‎on installing the Arduino IDE. If you have not previously installed an Arduino library, please check out ‎our installation guide.‎

The easiest way to install the library is to search for SparkFun Qwiic Button in the Arduino Library Manager ‎tool. You can also manually install the Qwiic Button Library from the GitHub Repository or you can download it ‎by clicking the button below.‎

DOWNLOAD THE SPARKFUN QWIIC BUTTON LIBRARY (ZIP)

Library Functions

Here is a list of the functions of the library with some quick descriptions of what they do. The examples cover ‎most of the functions, so we recommend going through them first.‎

Device Status

  • begin(uint8_t address = DEFAULT_ADDRESS, TwoWire &wirePort = Wire);- Sets device I2C address to a user-‎specified address, over whatever port the user specifies.
  • isConnected();- Returns true if the button will acknowledge over I2C, false otherwise.‎
  • uint8_t deviceID();- Return the 8-bit device ID of the attached device.
  • checkDeviceID();- Returns true if the device ID matches that of either the button or the switch
  • uint8_t getDeviceType();- Returns 1 if a button is attached, 2 if a switch is attached. Returns 0 if there is no ‎device attached.‎
  • uint16_t getFirmwareVersion();- Returns the firmware version of the attached device as a 16-bit integer. ‎The leftmost (high) byte is the major revision. The rightmost (low) byte is the minor version number. (Ex. ‎‎0x0202 is v2.02)‎
  • setI2Caddress(uint8_t address);- Configures the attached device to attach to the I2C bus using the specified ‎address.‎
  • uint8_t getI2Caddress();- Returns the I2C address of the device.‎

Note: The "setI2Caddress();" function will not work if any of the I2C address jumpers are closed. Assuming the ‎code is able to connect to the device, the library function may change the I2C address stored in EEPROM. ‎However, by default the firmware will stay at the alternate I2C jumper address and the last part of this ‎function won't be able to connect to the button for the firmware printout and future I2C address changes.‎

Button Status/Configuration

  • isPressed();- Returns 1 if the button is pressed, and 0 otherwise.‎
  • hasBeenClicked();- Returns 1 if the button was clicked, and 0 otherwise.
  • uint8_t setDebounceTime(uint16_t time);- Sets the time that the button waits for the mechanical contacts to ‎settle (in ms) and checks if the register was set properly. Returns 0 on success, 1 on register I2C write ‎fail, and 2 if the value didn't get written into the register properly.‎
  • uint16_t getDebounceTime();- Returns the value set to wait for the button's the mechanical contacts to ‎settle, (in ms).‎

Note: You may notice there are two button status functions listed: isPressed(); and hasBeenClicked();. ‎The isPressed(); function returns true while the button is pressed/held down and false when the button is ‎unpressed/released. The hasBeenClicked(); function will only return true when the button is pressed and ‎then released.‎

Interrupt Status/Configuration

  • uint8_t enablePressedInterrupt();- Configure the interrupt pin to go LOW while the button is pressed (held ‎down).‎
  • uint8_t disablePressedInterrupt();- Sets the interrupt to no longer trigger while the button is pressed.‎
  • uint8_t enableClickedInterrupt();- Configure the interrupt pin to go LOW when the button is clicked.‎
  • uint8_t disableClickedInterrupt();- Configures the interrupt pin to no longer go low when the button is clicked.‎
  • uint8_t clearEventBits();- Sets "isPressed", "hasBeenClicked", and "eventAvailable" to zero.‎
  • uint8_t resetInterruptConfig();- Resets all interrupt configuration settings back to defaults.‎

FIFO Queue

  • isPressedQueueFull();- Checks the queue of button press timestamps and returns true if full, false ‎otherwise.‎
  • isPressedQueueEmpty();- Opposite of the above function. Checks if the timestamp queue is empty.
  • unsigned long timeSinceLastPress();- Returns the time (in ms) since the last button press.‎
  • unsigned long timeSinceFirstPress();- Returns time (in ms) since the first button press.
  • popPressedQueue();- Returns the oldest value in the Pressed Queue (ms since first button press), and then ‎removes it.‎
  • isClickedQueueFull();- Checks the queue of button click timestamps and returns true if full, false otherwise.‎
  • isClickedQueueEmpty();- Opposite of the above function. Checks if the timestamp queue is empty.
  • unsigned long timeSinceLastClick();- Returns the time (in ms) since the last button click.‎
  • unsigned long timeSinceFirstClick();- Returns the time (in ms) since the first button click.
  • popClickedQueue();- Returns the oldest value in the Clicked Queue (ms since first button click), and then ‎removes it.‎

Button LED Configuration

  • LEDoff();- Turn the button LED off.‎
  • LEDon(uint8_t brightness = 255);- Turn the button LED on and set the brightness.‎
  • LEDconfig(uint8_t brightness, uint16_t cycleTime, uint16_t offTime, uint8_t granularity = 1);- Configures the button ‎LED.‎
    • Brightness: Stores the brightness of the LED. Accepts values between 0 and 255.‎
    • cycleTime: Total pulse cycle time (in ms). Does not include off time.‎
    • offTime: Off time between pulses (in ms). Default is 500 ms.‎
    • granularity: Amount of steps it takes to get to the set brightness level.‎

Internal I2C Abstraction

Advanced Functions! This list of functions is for reading/writing to one or more registers. They are beyond ‎the scope of this tutorial and are included primarily for users to implement in custom code.

  • uint8_t readSingleRegister(Qwiic_Button_Register reg); - Reads a single 8-bit register.
  • uint16_t readDoubleRegister(Qwiic_Button_Register reg); - Reads a 16-bit register (little endian).‎
  • unsigned long readQuadRegister(Qwiic_Button_Register reg); - Reads a 32-bit register (little endian).‎
  • writeSingleRegister(Qwiic_Button_Register reg, uint8_t data); - Attempts to write data into a single 8-bit ‎register. Does not check to make sure it was written successfully. Returns 0 if there was no error on I2C ‎transmission, and 1 otherwise.‎
  • writeDoubleRegister(Qwiic_Button_Register reg, uint16_t data); - Attempts to write data into a double (two 8-‎bit) registers. Does not check to make sure it was written successfully. Returns 0 if there was no error ‎on I2C transmission, and 1 otherwise.‎
  • uint8_t writeSingleRegisterWithReadback(Qwiic_Button_Register reg, uint8_t data); - Writes data into a single 8-‎bit register and checks to make sure the data was written successfully. Returns 0 on no error, 1 on I2C ‎write fail, and 2 if the register doesn't read back the same value that was written.‎
  • uint16_t writeDoubleRegisterWithReadback(Qwiic_Button_Register reg, uint16_t data); - Writes data into a double ‎‎(two 8-bit) registers and checks to make sure the data was written successfully. Returns 0 on no error, 1 ‎on I2C write fail, and 2 if the register doesn't read back the same value that was written.‎

Arduino Examples

In this section we will go over a few of the examples from our Qwiic Button Arduino Library. Here is a full list of ‎all the examples included in the library:‎

  • Example 1 - Prints the button status.‎
  • Example 2 - Turns the button LED on while the button is pressed.‎
  • Example 3 - Pulses the button LED while the button is pressed.‎
  • Example 4 - Demonstrates how to use the FIFO Queue and returns time elapsed since button presses.
  • Example 5 - Details how to identify and change the I2C address.
  • Example 6 - I2C Bus Configuration. Useful for devices with multiple I2C ports.‎
  • Example 7 - Sets up 2 Qwiic Buttons and reads their statuses.‎
  • Example 8 - Configures the button to toggle the interrupt pin when pressed.‎

Example 1: Print Button Status

The code for Example1_PrintButtonStatus connects the Qwiic Button to the I2C bus and prints the status of ‎the button (pressed or not pressed) to the Serial Monitor.‎

Example1_Animation

Example 3 Pulse When Pressed

Example3_PulseWhenPressed connects the Qwiic Button to the I2C bus and runs the Button LED through a ‎configured sequence when the button is pressed. The code configures the LED settings for brightness, ‎cycleTime and offTime to pulse the Button LED while it is pressed. Try playing around with these settings to ‎change the behavior of the LED.‎

Example 4 Queue Usage

Example4_QueueUsage demonstrates how to call, check, and alter the FIFO Queue for a button press and ‎button clicks. The code will check both the Pressed and Clicked queues and, if the queue is not empty, prints ‎over serial the time since the first press (since the queue was last cleared) and the time since the last press. ‎Entering "P" in the serial monitor will "pop" the Pressed Queue to return the oldest value stored in the queue ‎and then remove it. Entering "C" will perform the same action for the Clicked Queue.‎

Example 5 Change I2C Address

Heads up! This example will not change the I2C address if one of the address jumpers is closed. The Qwiic ‎Button will remain at the alternate address set by the address jumpers.‎

Example5_ChangeI2C Address checks to initialize the Qwiic Button on the I2C bus. If the device ID matches ‎what is expected (0x6F by default), it then will print some helpful information for changing the I2C address and ‎prompt you for an input to change the address. Once a new device ID is input and is valid, the code writes the ‎new I2C address to EEPROM on the ATtiny84 and prints out a success note along with the new device ID. If the ‎entered address is invalid or for some reason the write fails, the code will print out an error detailing what ‎failed.‎

If the device ID does not match what is expected, it runs a scan for devices on the bus and prints out the ID of ‎any attached device. Make sure to set up the Serial Monitor for the correct baud rate and enable both Newline ‎and Carriage Return. Also, do not enter the "0x" prefix. For example, you want to set the address to "0x5B", ‎type in "5B" and press enter. The gif below shows the serial printout of a successful initialization and device ‎address change to 0x5B:‎

Example5_Animation

Changing I2C Address Again: If you need to change the I2C address of your Qwiic button after altering it using ‎the above example, you will need to modify the button.begin(); function to include the alternate address. For ‎example, if the new address is 0x5B, your begin function should look like this: button.begin(0x5B);‎

Example 8 External Interrupt

Example8_ExtInterrupt demonstrates how to use the external interrupt pin to trigger an event on an ‎attached microcontroller. You will want to solder to the INT pin and connect it to an interrupt-capable pin. If ‎you just need to quickly prototype a circuit using the INT pin on the Qwiic Button, you can connect to it using ‎something like these IC Hooks. The photo below demonstrates how to use the IC Hook for a temporary ‎connection.‎

The code initializes the Qwiic Button on the I2C bus, attaches an interrupt to the selected pin (D2 by default), ‎and configures the interrupt function for any button event (pressed or clicked). The INT pin will go LOW ‎whenever a button event is registered and the selected interrupt pin on the microcontroller will fire whenever ‎it sees a FALLING edge (going from HIGH to LOW). If you want to see it in action, you could attach an LED to ‎the selected interrupt pin or you can modify the code to toggle all sorts of functions whenever the interrupt pin ‎goes LOW.‎

The example attaches an interrupt to D2 by default. This works fine for a RedBoard Qwiic or Arduino Uno but ‎may not work on other Arduinos. The Arduino attachInterrupt Reference Page will have a list of interrupt-‎capable pins for common Arduinos. Check that table or, if your chosen Arduino microcontroller is not on that ‎list, check the documentation for your specific microcontroller and adjust the int interruptPin = 2; call to the ‎appropriate I/O pin.‎

attaches_15

Register Map

If you would like to use a different development environment than Arduino, you can use the register map ‎below to communicate with the Qwiic Button.

maptable_16

You can also download the PDF.

The Qwiic Button behaves as a normal I2C device. First write the address of the register you would like to read ‎or write, then follow that I2C command with a Read to read the given register or a Write and a data byte to ‎write to a register.‎

Python Package

Note: This tutorial assumes you are using the latest version of Python 3. If this is your first time using Python ‎or I2C hardware on a Raspberry Pi, please checkout our tutorial on Python Programming with the Raspberry ‎Pi and the Raspberry Pi SPI and I2C Tutorial. Jetson Nano users can check out this tutorial on Working with ‎Qwiic on a Jetson Nano through Jupyter Notebooks.

We've written a Python package to easily get setup and use the Qwiic Button. There are two methods for ‎installing the Python package for the Qwiic Button.‎

  1. Install the all-inclusive SparkFun Qwiic Python package.
  2. Independently install the SparkFun Button Python package.‎

The all-inclusive SparkFun Qwiic Python package, is recommended as is also installs the required I2C driver as ‎well.‎

Note: Don't forget to double check that the hardware I2C connection is enabled on your single board computer.‎

SparkFun Qwiic Package

This repository is hosted on PyPi as the sparkfun-qwiic package. On systems that support PyPi installation ‎via pip3 (use pip for Python 2) is simple, using the following commands:‎

For all users (note: the user must have sudo privileges):‎

Copy Code
sudo pip3 install sparkfun-qwiic

For the current user:‎

Copy Code
pip3 install sparkfun-qwiic

Independent Installation

You can install the sparkfun-qwiic-button Python package independently, which is hosted by PyPi. However, if you ‎prefer to manually download and install the package from the GitHub repository, you can grab them here ‎‎(*Please be aware of any package dependencies. You can also check out the repository documentation page, ‎hosted on ReadtheDocs.):‎

DOWNLOAD THE SPARKFUN QWIIC BUTTON PYTHON PACKAGE (ZIP)‎

PyPi Installation

This repository is hosted on PyPi as the sparkfun-qwiic-button package. On systems that support PyPi installation ‎via pip3 (use pip for Python 2) is simple, using the following commands:‎

For all users (note: the user must have sudo privileges):‎

Copy Code
sudo pip3 install sparkfun-qwiic-button

For the current user:‎

Copy Code
pip3 install sparkfun-qwiic-button

Local Installation

To install, make sure the setuptools package is installed on the system.‎

Direct installation at the command line (use python for Python 2):‎

Copy Code
python3 setup.py install

To build a package for use with pip3:‎

Copy Code
python3 setup.py sdist

A package file is built and placed in a subdirectory called dist. This package file can be installed using pip3.‎

Copy Code
cd dist
pip3 install sparkfun_qwiic_button-<version>.tar.gz

Python Package Operation

Before we jump into getting readings, let's take a closer look at the available functions in the Python package. ‎Below, is a description of the basic functionality of the Python package. This includes the package organization, ‎built-in methods, and their inputs and/or outputs. For more details on how the Python package works, check ‎out the source code and package documentation.‎

Dependencies

This Python package has a very few dependencies in the code, listed below:‎

Copy Code
import qwiic_i2c
import math

Default Variables

The default variables, in the code, for this Python package are listed below:

Copy Code
# qwiic_button GLOBAL VARIABLES
#----------------------------------------------------------------------------------------------------
# Define the device name and I2C addresses. These are set in the class defintion
# as class variables, making them avilable without having to create a class instance.
# This allows higher level logic to rapidly create a index of qwiic devices at
# runtine
#
# The name of this device
_DEFAULT_NAME = "Qwiic Button"

# Some devices have multiple available addresses - this is a list of these addresses.
# NOTE: The first address in this list is considered the default I2C address for the
# device.
_AVAILABLE_I2C_ADDRESS = [0x6F]

Note: This package is different from the previous packages as the register variables are declared in the object class.

Copy Code
# QwiicRFID CLASS VARIABLES
#----------------------------------------------------------------------------------------------------
# Device ID for all Qwiic Buttons
DEV_ID = 0x5D

# Registers
ID = 0x00
FIRMWARE_MINOR = 0x01
FIRMWARE_MAJOR = 0x02
BUTTON_STATUS = 0x03
INTERRUPT_CONFIG = 0x04
BUTTON_DEBOUNCE_TIME = 0x05
PRESSED_QUEUE_STATUS = 0x07
PRESSED_QUEUE_FRONT = 0x08
PRESSED_QUEUE_BACK = 0x0C
CLICKED_QUEUE_STATUS = 0x10
CLICKED_QUEUE_FRONT = 0x11
CLICKED_QUEUE_BACK = 0x15
LED_BRIGHTNESS = 0x19
LED_PULSE_GRANULARITY = 0x1A
LED_PULSE_CYCLE_TIME = 0x1B
LED_PULSE_OFF_TIME = 0x1D
I2C_ADDRESS = 0x1F

# Status Flags
event_available = 0
has_been_clicked = 0
is_pressed = 0

# Interrupt Configuration Flags
clicked_enable = 0
pressed_enable = 0

# Pressed Queue Status Flags
pressed_pop_request = 0
pressed_is_empty = 0
pressed_is_full = 0

# Clicked Queue Status Flags
clicked_pop_request = 0
clicked_is_empty = 0
clicked_is_full = 0

Class

QwiicButton() or QwiicButton(address)

This Python package operates as a class object, allowing new instances of that type to be made. ‎An __init__() constructor is used that creates a connection to an I2C device over the I2C bus using the default or ‎specified I2C address.‎

The Constructor

A constructor is a special kind of method used to initialize (assign values to) the data members needed by the ‎object when it is created.‎

‎__init__(address=None, i2c_driver=None):‎

Input: value

The value of the device address. If not defined, the Python package will use the default I2C address (0x6F) ‎stored under _AVAILABLE_I2C_ADDRESS variable.‎

Input: i2c_driver

Loads the specified I2C driver; by default, the Qwiic I2C driver is used: qwiic_i2c.getI2CDriver(). Users should use ‎the default I2C driver and leave this field blank.‎

Functions

A function is an attribute of the class, which defines a method for instances of that class. In simple terms, they ‎are objects for the operations (or methods) of the class. A list of all the available functions are detailed on ‎the API Reference page of ReadtheDocs for the Qwiic_Button_Py Python package.

‎Upgrading the Python Package

In the future, changes to the Python package might be made. Updating the installed packages has to be done ‎individually for each package (i.e., sub-modules and dependencies won't update automatically and must be ‎updated manually). For the sparkfun-qwiic-button Python package, use the following command (use pip for ‎Python 2):‎

For all users (note: the user must have sudo privileges):‎

Copy Code
sudo pip3 install --upgrade sparkfun-qwiic-button

For the current user:‎

Copy Code
pip3 install --upgrade sparkfun-qwiic-button

Python Examples

Note: Work on this section is in progress. We will update the content as soon as we can.‎

Resources and Going Further

For more information, check out the resources below:‎

Need help getting started with Arduino and I2C? Check out these resources:‎

Herst.-Teilenr. 15932
SPARKFUN QWIIC BUTTON - RED LED
SparkFun Electronics
Herst.-Teilenr. 16842
SPARKFUN QWIIC BUTTON - GREEN LE
SparkFun Electronics
Herst.-Teilenr. 15931
SPARKFUN QWIIC BUTTON BREAKOUT
SparkFun Electronics
Herst.-Teilenr. 15123
REDBOARD QWIIC ATMEGA328 EVAL BD
SparkFun Electronics
Herst.-Teilenr. 15663
SPARKFUN THING PLUS ESP32 WROOM
SparkFun Electronics
Herst.-Teilenr. 15444
REDBOARD ARTEMIS
SparkFun Electronics
Herst.-Teilenr. 15423
SAMD21 QWIIC MICRO DEV BOARD
SparkFun Electronics
Herst.-Teilenr. 14427
QWIIC CABLE - 100MM
SparkFun Electronics
Herst.-Teilenr. 17257
FLEXIBLE QWIIC CABLE - 500MM
SparkFun Electronics
Herst.-Teilenr. 14495
QWIIC ADAPTER
SparkFun Electronics
Herst.-Teilenr. 14352
QWIIC SHIELD FOR ARDUINO
SparkFun Electronics
Herst.-Teilenr. 14425
QWIIC CABLE - BREADBOARD JUMPER
SparkFun Electronics
Herst.-Teilenr. 17261
FLEXIBLE QWIIC CABLE - FEMALE JU
SparkFun Electronics
Herst.-Teilenr. 09190
SWITCH TACTILE SPST-NO
SparkFun Electronics
Herst.-Teilenr. 09163
SOLDER LEAD FREE - 15-GRAM TUBE
SparkFun Electronics
Herst.-Teilenr. 14681
SPARKFUN BEGINNER TOOL KIT
SparkFun Electronics
Herst.-Teilenr. 14460
MULTICOLOR BUTTONS - 4-PACK
SparkFun Electronics
Herst.-Teilenr. K000007
STARTER KIT W/ARDUINO BOARD
Arduino
Add all DigiKey Parts to Cart
Have questions or comments? Continue the conversation on TechForum, DigiKey's online community and technical resource.