Maker.io main logo

Oscilloscope Clock Simulation on a Round ESP32 Display

80

2026-02-16 | By Mirko Pavleski

License: General Public License Real Time Clocks (RTCs) ESP32

An oscilloscope clock is a circuit that turns an old analog oscilloscope into a stylish, retro-themed clock. A Cathode Ray Tube (CRT) displays a clock face—either digital or analog—using the screen's ability to draw lines based on voltage. The "X" (horizontal) and "Y" (vertical) inputs of the oscilloscope are controlled by the circuit, and by rapidly changing these voltages, the circuit "draws" numbers or clock hands on the screen. In one of my previous projects, I presented the simplest way to make such a clock yourself.

hjiu

However, its construction requires relatively solid knowledge in the field of electronics and high voltage, and it's also quite expensive.

njk

This time, I will show you an extremely simple way to make an "oscilloscope clock" on an Elecrow 2.1-inch Crowpanel circular display that completely visually imitates the original. Starting from the circular shape of the display, through the original green color, the marked scale, up to the shape, and the way the lines are displayed and illuminated, it irresistibly reminds one of a CRT tube.

It is also desirable to mount it in a suitable housing that would resemble a retro CRT oscilloscope for the effect to be maximum.

So, to make this clock, no soldering or external components are required. The round display contains a built-in ESP32S3 microcontroller with Wi-Fi and Bluetooth capabilities. We only need to upload the given code, and the device is ready in a few minutes. But before that, certain settings should be noted.

First, you need to use Arduino IDE version 1.8.15 or later. Then you need to install the newest ESP32 Core. Now in Tools-Board-ESP32 Arduino, we need to select ESP32S3 Dev Module. In this board, we need to make several changes to the properties:

  • Flash Size: 16MB

  • Partition scheme: Huge App

  • PSRAM: OPI PSRAM.

gjhg

You also need to install the Arduino_GFX_Library. Now we can compile and upload the code without errors. As for the code, the basic settings are located at the beginning; here, you need to insert the Wi-Fi credentials, the NTP server, and the definition of the display colors.

hgjigh

Now let's see how the device works in real conditions. Immediately after turning on, the clock connects to the Wi-Fi network and gets the correct time from the NTP server. Then an analog clock appears on the display in the style of an oscilloscope clock with a characteristic green color. Even a "glow" effect has been added when drawing the characters, but unfortunately, it is almost not noticeable in the video recording. To make it even closer to the original, I added an option to change the dimensions of the clock using the rotary encoder that is part of the display module.

ghyuig

In this way, it simulates a change in the amplitude of the signals fed to the X and Y inputs on the original oscilloscope. By pressing the display (the button on the rotary encoder), a digital oscilloscope clock is activated, drawn with arcs and straight lines, which is characteristic of the original oscilloscope version. Here, as before, I introduced a "glow" effect. By pressing again, we return to the analog clock. As for the digital clock, in the first version of the code, the content was formed only by drawing straight lines, which is also characteristic of these devices. At the end of the text, both versions of the code are given.

yguiyhi

And finally, a short conclusion. By combining the vintage aesthetics of a CRT oscilloscope with modern ESP32 hardware, this project proves you don't need dangerous high voltage to enjoy the classic look of a vector clock. It’s the perfect weekend project for any maker looking to add some retro flair to their desk.

Have questions or comments? Continue the conversation on TechForum, DigiKey's online community and technical resource.