High Power LEDs : 500 mA - 999 mAThis section contains discrete LEDs with current ratings from 500 mA to 999 mA. The LEDs are subdivided by wavelength into color groups. To use this section, select a color from one of the options below and click on the Compare Product Specifications link. In addition, specific products are listed below for each color category.
A second option is the
Parametric Search which can be used to view all LEDs in this section.
-
Warm White
-
Neutral White
-
Cool White
-
Blue
-
Green
-
Yellow
-
Orange
-
Red
|
Warm White
|
These LEDs have a correlated color temperature between 2500 K and 3699 K which correspond to the visible colors generally classified as warm white. These color temperatures are outlined on the C.I.E. Diagram.
|
Avago - Moonstone
|
Avago 3W Moonstone™ Power LED series is available in Cool White & Warm White colors. The exposed pad design has excellent heat transfer from the package to the motherboard which allows high driving currents.
|
|
Pricing & Availability
|
Cree, Inc. - XP-E
|
The XLamp MC-E LED is a lighting-class multi-chip LED that provides 4 times the flux as XLamp XR-E in the same footprint, without compromising thermal performance. XLamp MC-E reduces LED system cost by reducing system complexity and the number of components required.
|
|
Pricing & Availability
|
|
Neutral White
|
These LEDs have a correlated color temperature between 3700 K and 4999 K which correspond to the visible colors generally classified as neutral white. These color temperatures are outlined on the C.I.E. Diagram.
|
Cree - XR-C
|
The XLamp XR-C LED gives lighting designers the flexibility and performance to create the next generation of LED lighting products. XLamp XR-C LEDs feature electrically neutral thermal path, low thermal resistance and support for a wide range of drive currents.
|
|
Pricing & Availability
|
OSRAM - Platinum Dragon
|
The Platinum Dragon family offers a full white color spectrum and a broad portfolio. The thermal resistance is 9 K/W (typ) which allows a maximum forward current of 1 A and a surge current of 2.5 A. This family is fully reflow solderable and has a maximum junction temperature of 125°C. The radiation characteristics are well suited for secondary optics.
|
|
Pricing & Availability
|
|
Cool White
|
These LEDs have a correlated color temperature between 5000 K and 8000 K which correspond to the visible colors generally classified as cool white. These color temperatures are outlined on the C.I.E. Diagram.
|
Cree, Inc. - XR-C
|
The XLamp XR-C LED gives lighting designers the flexibility and performance to create the next generation of LED lighting products. XLamp XR-C LEDs feature electrically neutral thermal path, low thermal resistance and support for a wide range of drive currents.
|
|
Pricing & Availability
|
Cree, Inc. - XP-C
|
The XLamp XP-C LED combines the proven lighting-class performance and reliability of the XLamp XR-E LED in a package with 80% smaller footprint. The XLamp XP-C LED continues Cree’s history of innovation in LEDs for lighting applications with wide viewing angle, symmetrical package, unlimited floor life and electrically neutral thermal path.
|
|
Pricing & Availability
|
|
Blue
|
These LEDs have wavelengths between 428 nm and 491 nm which correspond to visible colors in the blue spectrum as shown on the C.I.E. Diagram.
|
Cree, Inc. - XR-C
|
The XLamp XR-C LED gives lighting designers the flexibility and performance to create the next generation of LED lighting products. XLamp XR-C LEDs feature electrically neutral thermal path, low thermal resistance and support for a wide range of drive currents.
|
|
Pricing & Availability
|
|
Green
|
These LEDs have wavelengths between 492 nm and 575 nm which correspond to visible colors in the green spectrum as shown on the C.I.E. Diagram.
|
Cree, Inc. - XR-E
|
The XLamp XR-E LED is leading the LED lighting revolution with its unprecedented lighting-class brightness, efficacy, lifetime and quality of light. These lighting-class features enable the XLamp XR-E LED to replace many traditional light sources and save money with energy-efficient light and long lifetimes.
|
|
Pricing & Availability
|
Cree, Inc. - XR-C
|
The XLamp XR-C LED gives lighting designers the flexibility and performance to create the next generation of LED lighting products. XLamp XR-C LEDs feature electrically neutral thermal path, low thermal resistance and support for a wide range of drive currents.
|
|
Pricing & Availability
|
|
Yellow
|
These LEDs have wavelengths between 576 nm and 596 nm which correspond to visible colors in the yellow spectrum as shown on the C.I.E. Diagram.
|
Cree, Inc. - XP-E
|
The XLamp XP-E LED combines the proven lighting-class performance and reliability of the XLamp XR-E LED in a package with 80% smaller footprint. The XLamp XP-E LED continues Cree’s history of innovation in LEDs for lighting applications with wide viewing angle, symmetrical package, unlimited floor life and electrically neutral thermal path.
|
|
Pricing & Availability
|
OSRAM - Platinum Dragon
|
The Platinum Dragon family offers a full white color spectrum and a broad portfolio. The thermal resistance is 9 K/W (typ) which allows a maximum forward current of 1 A and a surge current of 2.5 A. This family is fully reflow solderable and has a maximum junction temperature of 125°C. The radiation characteristics are well suited for secondary optics.
|
|
Pricing & Availability
|
|
Orange
|
These LEDs have wavelengths between 597 nm and 619 nm which correspond to visible colors in the orange spectrum as shown on the C.I.E. Diagram.
|
OSRAM - Platinum Dragon
|
The Platinum Dragon family offers a full white color spectrum and a broad portfolio. The thermal resistance is 9 K/W (typ) which allows a maximum forward current of 1 A and a surge current of 2.5 A. This family is fully reflow solderable and has a maximum junction temperature of 125°C. The radiation characteristics are well suited for secondary optics.
|
|
Pricing & Availability
|
|
Red
|
These LEDs have wavelengths between 620 nm and 780 nm which correspond to visible colors in the red spectrum as shown on the C.I.E. Diagram.
|
Cree, Inc. - XR-C
|
The XLamp XR-C LED gives lighting designers the flexibility and performance to create the next generation of LED lighting products. XLamp XR-C LEDs feature electrically neutral thermal path, low thermal resistance and support for a wide range of drive currents.
|
|
Pricing & Availability
|
OSRAM - Platinum Dragon
|
The Platinum Dragon family offers a full white color spectrum and a broad portfolio. The thermal resistance is 9 K/W (typ) which allows a maximum forward current of 1 A and a surge current of 2.5 A. This family is fully reflow solderable and has a maximum junction temperature of 125°C. The radiation characteristics are well suited for secondary optics.
|
|
Pricing & Availability
|
|